Cancel
Showing results for 
Search instead for 
Did you mean: 

"Update on file save" batch switch on

Legend
Legend

Hi,

 

A very, very long time ago we finally got  the possibility to update the mass of an assy on save..and thus display the correct mass on a drawing.

 

Save as.jpg

Since I have a lot old files still in use, the switch is default off when I open these files, and thus the mass could be incorrect.

 

Is there a a way to change this behaviour.

 

I would like to switch this on by default, even if the file is created in a version where this option was not available.

 

or

 

is there a batch tool that could do this job, open the old file, switch it on, and close it again.

 

Your input is greatly appreciated.

 

Kind Regards,

 

 

Jan Bos

Emmen, The Netherlands

User since Solid Edge V3.5

 

 

 

 

1 REPLY 1

Betreff: "Update on file save" batch switch on

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi @Jan_Bos,

it should be possible to integrate that line into the OpenSave macro.
regards
Wolfgang