Cancel
Showing results for 
Search instead for 
Did you mean: 

rectangle

Creator
Creator

I want to create diagonal of rectangle every time when i draw rectangle with center rectangle.

is it possible in solidworks

 

2 REPLIES

Re: rectangle

Phenom
Phenom

Hi @Raumik

 

I am a former SW user, I understand your habits.

 

No you cannot draw diagonal lines automatically. You can create them separatelly drawing them.

 

For your better sleep I would suggest to leave you SW habits home and focus to learn SE from scratch.

I was frustrated as you at the begining but every CAD is worth to learn , especially SE - which after my experience is a better ONE.

 

Enjoy !

Arek

Highlighted

Re: rectangle

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Agree with what @arekkul said.

  

For just this case, try the Rectangle-Centerlines macro which works in both Draft and Sketcher, 

available from my download page:

http://www.cadvertex.com/download.htm

  

1. It is the third in the Free Apps list.

2. A video is also available next to the download.

3. The download zip also contains an image which you can use on a button on the ribbon.

4. A detailed tutorial on how the program was coded is also available here:

http://www.surfandcode.in/2014/01/index-of-all-tutorials-on-this-solid.html

5. Scroll down to the 3rd topic under MakerFaire section.

  

6. If you need, here's a link to the steps on how to add the macro to a ribbon button using the provided image for the button in Solid Edge:

http://www.surfandcode.in/2015/07/running-macro-from-ribbon-button.html

  

Hope you like the macro and also find it useful.

  

7. If you are on FaceBook, join the Solid Edge user's group mentioned below - there were 776 Solid Edge topics last year alone.

  

~Tushar Suradkar

fb.pngSolid Edge Users Facebook Group - Let's Sync

 

Finally I could not resist posting the UI of the program:

Isin't it more feature rich than the one in SolidWorks ?

 

RCen.png