Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

reviste draft template

Experimenter
Experimenter

Has any one tried to change/upgrade or revise the template of a batch of drawings?

I have a lots of draft tiles that use different templates for different companies. Now a new template that meges all the previous templates into one single template document. Now, I want to reivse all those drawings to have the new template so I can choose what sheet and title block to use as I can do with my new template.

 

Please if I wasn't clear, let me know I would really like to know the opinion of the community.

 

Regards

 

Vic.  

3 REPLIES 3

Re: reviste draft template

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This can be done through automation and there are a couple of visual basic utilities some folks have written to do this.  If you are using the "Free" version, I believe that the API needed to use custom code is not accessible.  If you are using the "commercial" version (Solid Edge 2D - you had to purchase a license/maintenance), then it will have a usable API.

 

Search in the Solid Edge Forum for "replace background" and you should find them.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: reviste draft template

Siemens Phenom Siemens Phenom
Siemens Phenom

FYI, in ST9 there is a new "Replace Background" command that although it does not allow you to do en masse changes, it will greatly ease the process for changing the background sheet manually.

Re: reviste draft template

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And since there is also an API for it, it could simplify the automation of a bulk change process as well Smiley Happy



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com