Cancel
Showing results for 
Search instead for 
Did you mean: 

saving and e mailing prints

Experimenter
Experimenter

I have the free 2d software,can i save and e mail drawings in a pdf format. If how?

4 REPLIES

Re: saving and e mailing prints

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If it is in Free 2D, just do a Save As and change the Save As Type to PDF.  Then save to folder and then e-mail.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: saving and e mailing prints

Experimenter
Experimenter

Thank you,I'll give that a shot.

Re: saving and e mailing prints

Valued Contributor
Valued Contributor

Hi Jason

As far as I know frees2D doesn't support "save as pdf".

However there is an easy solution. Download some freeware such as pdfcreator, this is a pseudo printer.

To create a pdf click print, then chose pdfcreator from the list of available printers, then instead of a hardcopy you get a pdf.

I use this method everday and it works a treat. There are many different freeware packages if you don't like pdfcreator.

 

Cheers

Pete

 

 

Re: saving and e mailing prints

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It's possible Windows 10 already has a "Microsoft Print to PDF" option when printing.  I have it but not sure if it came with Win 10 or Office 365/2016.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com