Cancel
Showing results for 
Search instead for 
Did you mean: 

setting up relations

Experimenter
Experimenter
using st9 2d drafting free edition i am trying to set up relations on a 6 x 91 inch front rail. the rail has three slots in it that i am trying to drive the locations when the length of the rail changes (91 inches). i set up the formulas in the variable table. i have tried every relationship i can and still cannot get this right. could someone take a look at the relationships i have and let me know what i did wrong or correct it and repost it so can study it. i have read and read on the relationships and tried for 2 days changing everything i could. i have been playing with this program for a month, so still a newbie thanks for any help
2 REPLIES 2

Re: setting up relations

Gears Phenom Gears Phenom
Gears Phenom

6-20-2017 7-53-04 AM.png

looks like you are missing a horizontal/Vertical relationship on your 2 lenghts (top and bottom)


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: setting up relations

Experimenter
Experimenter

thank you very much for the help. will keep studing, lol