Cancel
Showing results for 
Search instead for 
Did you mean: 

shaded view obscuring other shaded views when printing.

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

shaded.jpgHi Edgers

I'm pretty sure this is an old issue, but can't seem to find the reference to the fix. When printing (ST10 MP3), the boudaries of shaded views obscure other views on the sheet (see image). I know that you can manually change the boundary to stop this happening, but is there an easy way or a setting that can be set to fix this from happening?

This is a scan of an actual printed file, not a pdf.

 

 

7 REPLIES

Re: shaded view obscuring other shaded views when printing.

Phenom
Phenom

Save As > Save As Translated.

Set the type to pdf.

Click 'Options'

Tick the 'Transparent Drawing View Backgrounds' box.

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.

Re: shaded view obscuring other shaded views when printing.

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Does this work with a physically printed paper copy or just the pdf? As I said in my post, this image is a scan copy of a paper print, not a pdf.

Re: shaded view obscuring other shaded views when printing.

Phenom
Phenom

@beachcombers solution changes the PDF produced, and hence the printout. You'll have to re-export the PDF from SE to 'fix' the existing ones.

Re: shaded view obscuring other shaded views when printing.

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Thanks. So the answer is no, as it is not printing to a printer, but to a pdf. The process of printing to pdf and then printing the pdf is still extra steps.

Highlighted

Re: shaded view obscuring other shaded views when printing.

Gears Phenom Gears Phenom
Gears Phenom

you can manually edit the view boundary shape...   this is my preference.


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Betreff: shaded view obscuring other shaded views when printing.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Alan

 

 

 

see the linked post from a time ago.

The printing with shaded views is an issue for years now.

 

The shown registry entry helped in the past.

 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Shaded-print-error-on-HP5200/m-p/44...

 

 

regards
Wolfgang

Betreff: shaded view obscuring other shaded views when printing.

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Thanks, I'll give that a go.