Cancel
Showing results for 
Search instead for 
Did you mean: 

sheet Metal Coversion...

Valued Contributor
Valued Contributor

Hello Edge Users ...

The following file was created by someone using nx to model SheetMetal.
I want to import this file to Edge and convert it to sheet metal.
It does not work.
Do you know what's wrong?

 

ss.png

12 REPLIES 12

Betreff: sheet Metal Coversion...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

the problem seems to occur due to the in accuracy of the translation

 

See picture showing You the difference in thickness 

 

20170515_0950.PNG

 

 

 

You easily can repair this using the Optimize function of Inspect Tools

 

20170515_1003.PNG

 

 

After repairing You can create Your sheet metal part using the "Thin Part To Sheet Metal" button in ordered mode. Sync will not do this in Yopur case, since there seems to be connections radius to radius which arenot working in sync but do it in ordered.

 

 

See flatten pattern

 

20170515_1007.PNG

 

regards
Wolfgang

Betreff: sheet Metal Coversion...

Valued Contributor
Valued Contributor

There is a slight difference in thickness.
Thank you for suggesting a solution.
I did not know.
Thank you.

Betreff: sheet Metal Coversion...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

Yes but as said before, You need not changing anything here. Still run the Optimize command from Inspect tab.

This is all You have to do and then change it to Sheet Metal in Ordered!

 

 

regards
Wolfgang
Highlighted

Betreff: sheet Metal Coversion...

Valued Contributor
Valued Contributor

HI~ hawcad

I have an answer.
I can not optimize to reflect anything.
Do you know what will change when you optimize?

I am not good.
Could you please explain it again?

Betreff: sheet Metal Coversion...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

hi @Hclee

 

 

I cann't say what You miss but the Optimize command should be available to every one with every license.

 

I hav eattached the repaired and converted PSM uner 1#A.psm

 

 

regards
Wolfgang

Betreff: sheet Metal Coversion...

Valued Contributor
Valued Contributor

Oh, it's fixed.
I knew exactly what the optimization function was.
Thank you. Haw cad .. I love you ~~ ^^

Betreff: sheet Metal Coversion...

Gears Phenom Gears Phenom
Gears Phenom

Hi Hclee,

 

After optimisation you should get the Report with all changes After

 

OPT.png

 

regards,

 

Arek

Betreff: sheet Metal Coversion...

Valued Contributor
Valued Contributor

Thank you.

Betreff: sheet Metal Coversion...

Gears Phenom Gears Phenom
Gears Phenom

Hi Hclee,

 

to be more precise I have overlayedoverlay.png one to another and have changed the colour of the one to visualize what has changed,

 

Regards,

 

Arek