Cancel
Showing results for 
Search instead for 
Did you mean: 

sheetmetal part-full radius

Gears Phenom Gears Phenom
Gears Phenom

I occasionally work with a part that has a full radius (20") and start with a contour flange and then trim all edges to mating (to be welded) edges. I add small .050 "tabs" that are half radi to the edges to aid in mating the parts for welding. On a full radius part i need to unbend it to add these. no big deal typically but on a part that has no original edges to select to be the base. My work around has been to crate a cutout that has a straight edge to select.  Then i can unbend add my tabs then fill hole and rebend..  Seems unneccesary though.

-Craig
2 REPLIES 2

Re: sheetmetal part-full radius

Gears Phenom Gears Phenom
Gears Phenom

here's an image..1.jpg

-Craig

Re: sheetmetal part-full radius

Gears Phenom Gears Phenom
Gears Phenom

same file name but with the added cutout and tab for locating..

-Craig