Cancel
Showing results for 
Search instead for 
Did you mean: 

sketch relation

Creator
Creator

is it any way 

to attach midpoint of vertical line will attach to horizontal line without giving the dimensions

also i cant select the endpoint of those line in the sketch

3 REPLIES

Re: sketch relation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes. Pick the connect relation, pick the middle of the vertical line, then pick anywhere along the horizontal line.

And, for the endpoint selection make sure your intellisketch settings include endpoints:

IntellisketchSettings.JPG

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: sketch relation

Legend
Legend

You can click the connect button on the upper left, and then pick center of line to connect to other line.

 

Capture.PNG

Re: sketch relation

Community Manager Community Manager
Community Manager

Let me also give an "expert tip" to remember the MICE keys. When you are placing or modifying objects you can hit the keys on the keyboard to get that keypoint M=Midpoint E = Endpoint, you get the idea.

 

So when placing a line and you want to connect to the midpoint of another line, just hover over it and hit the M key --> Voila!

 

This works with the connect constraint as well. Choose the connect command. Hover over line one and hit M. Hover over line 2 and hit E and.....

 

Best,

Dan

Dan Staples
Director, Solid Edge Product Development