.sldprt default

Legend
Legend

Is there any way to set SE to open an SW part file by default?

Using SE since V12, 2002
2 REPLIES

Re: .sldprt default

Esteemed Contributor
Esteemed Contributor

SE retains the last file type open so it should stay at Solidworks Part Document until you select something else. Of course you still have to select an SE template after opening a non-native SE type.

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200

Re: .sldprt default

Esteemed Contributor
Esteemed Contributor

Hi Larry,

 

You can assign the default "open with" to the "Edge.exe" to open automatically in SE.....works for me.

 

[alternatively...assign the "SW2SE.exe", if you don't want to have confusingly similar icons to other SE assignments.....like DXF/DWG, etc....]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000