Cancel
Showing results for 
Search instead for 
Did you mean: 

soilid edge hangs.

N/A

i installed it corrctly. but as i staterd solid edge it hangs. i check the system requirement . it is ok . i installed it again. nothing happened the problem remains the same. my system configuration is
4 gb ram
win 7 64 bit
i gb graphic card .
pls do suggest what should i do.

1 REPLY

Re: soilid edge hangs.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Which version of Windows 7?
Sent from my Motorola Electrify using Tapatalk 2


Ken

Production: ST10 MP6
Testing: SE 2019