Cancel
Showing results for 
Search instead for 
Did you mean: 

solid edge v20 error

Experimenter
Experimenter

im using solid edge v20 when ever i try to use curve by table command i get this error "microsoft excel is not loaded this command cannot execute".Can any one tell me how to import coordinated form excel?

3 REPLIES 3

Re: solid edge v20 error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

Sounds like you do not have MS-Excel installed on the PC running Solid Edge....it is a requirement, to run features such as this one.

 

 

Also, you'd be better off posting things related to Solid Edge in that forum.....to ge a wider audience for your questions, etc.

 

http://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/bd-p/solid-edge-forum

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: solid edge v20 error

Experimenter
Experimenter

i have ms office 2013 installed. Can this error occur due to the installed  location of there softwares?

Re: solid edge v20 error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have not tried this, but I would assume so......I'd expect all applications to be installed on the windows drive, usually designated "C:"

Other than this, I'm not sure how to help.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000