Cancel
Showing results for 
Search instead for 
Did you mean: 

solidedge

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

can anybody know me what are the capabilities of solid edge Foundation & solid edge classic in terms of simulation also like to know can we do fatigue simulation in premium ??

6 REPLIES 6

Betreff: solidedge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Rahulk

 

 

 

this IMHO seems to be an easy answer.

 

With Foundation there is no Simulation included in Solid Edge.

Classic has the Simulation Express module with it, where the capabilities are rather limited.

Simulation only is possible for a single part with limited linear analysis of stress and natural frequency

 

Only force and pressure is possible as load, no connection due to no simulation in ASM

 

Also the post processing features are not to high.

 

This together makes the difference to Premium

 

 

regards
Wolfgang

Betreff: solidedge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Rahulk  Just to expand on what @hawcad mentioned, you can add a Simulation license to Classic without purchasing Premium which comes with Simulation.

 

I do not believe Simulation can do fatigue analysis.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Betreff: solidedge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

 

 

Yes, thanks for this additional info about Simulation as stand alone module for SE.

 

The only reason why I didn't mention this is, that the price for Simulation only is much higher than for an Premium Upgrade.

So therefore I recomment to upgrade rather than by the Simulation alone.

Wether or not You will use xPresRoute and Harness design, You will have them too.

 

regards
Wolfgang

Betreff: solidedge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcadFor us, we use floating licensing and only need a handful of Simulation or XpressRoute so we have a few licenses of each for our ~150 users.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Betreff: solidedge

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Thanks a lot, both of you! 

if we compare with Solidworks simulation as they use to propose SolidWorks professional ( cad)with SolidWorks simulation standard for motion, fatigue simulation. for such kind of prospect who is looking for SE cad at classic level & motion & fatigue simulation what should we propose?

Betreff: solidedge

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter
if we compare with Solidworks simulation as they use to propose SolidWorks professional ( cad)with SolidWorks simulation standard for motion, fatigue simulation. for such kind of prospect who is looking for SE cad at classic level & motion & fatigue simulation what should we propose?