Cancel
Showing results for 
Search instead for 
Did you mean: 

squeeze tube

Phenom
Phenom

For a project we will use round tube (dia 13mm x 1,5mm).

This tube needs to be 'squeezed' (pressed/flatten, I don't know how to tell this in Englisch) on different places.

After that we need to create a slot in the flat part of the tube.

 

Do I need to work with a sweep to simulate this or can I simply squeeze the tube with a single command?

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user
2 REPLIES 2

Re: squeeze tube

Hi Joris, so far I know this must be done with indeed the sweep command.
-------
Daniël Schuiling

Re: squeeze tube

Gears Phenom Gears Phenom
Gears Phenom

There is not command to "chrush" the end of that tube.  you mention Sweep...  but i beleivbe you will find LOFT to be a better command to transition between two different cross sections. (round to oval)

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7