04-03-2018 10:13 AM
Hi,
I have a solid edge premium licence , and i'm using Solidedge via cloud gateway.
How do i install standart parts database ?
Thanks in advance for your feedback
Solved! Go to Solution.
04-03-2018 10:33 AM
Hi @LaurentP
I would like to say, that You will have to install Standard Parts in the same way as with any other license typ.
I don't believe that the license You are using will influence the installation of the software.
So start with the Standard Parts Admin from the basic installation image - don't forget to have example parts turned ON, and then install the Machinery Library from the extra image.
After that You have to add wanted parts into the SQL database using the DB Admin
04-03-2018 10:47 AM
thanks for your answer @hawcad
You are talking about "installation image" , but i don't have any media.
I installed solid edge through Solid_Edge_Web_Installer and then activated my webkey account in solidedge.
so my main issue is, i guess, where can i download the media
04-03-2018 11:45 AM
Hi @LaurentP
if You have a web account, can You go to the dwonload area of the GTAC server?
04-03-2018 12:59 PM
when i try to connect to:
Training & Support / GTAC Siemens PLM / Download Server /WebKey Login Site
i got this message :
"Your WebKey account is valid, but you are not allowed access to this server."
it's probably a bad news ......
04-03-2018 01:08 PM
Hi @LaurentP
so maybe somebody from Siemens can clarify and explain how this is working?
It would be interesting how different license types are handled and what could be done by who.