Cancel
Showing results for 
Search instead for 
Did you mean: 

standart part installation using cloud installation

Creator
Creator

Hi,

 

I have a solid edge premium licence , and i'm using Solidedge via cloud gateway.

 

How do i install standart parts database ?

 

Thanks in advance for your feedback

5 REPLIES

Betreff: standart part installation using cloud installation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @LaurentP

 

 

 

I would like to say, that You will have to install Standard Parts in the same way as with any other license typ.

I don't believe that the license You are using will influence the installation of the software.

 

So start with the Standard Parts Admin from the basic installation image - don't forget to have example parts turned ON, and then install the Machinery Library from the extra image.

 

After that You have to add wanted parts into the SQL database using the DB Admin

 

 

regards
Wolfgang

Betreff: standart part installation using cloud installation

Creator
Creator

thanks for your answer @hawcad

 

You are talking about "installation image" , but i don't have any media.

I installed solid edge through Solid_Edge_Web_Installer and then activated my webkey account in solidedge.

so my main issue is, i guess, where can i download the media

 

Betreff: standart part installation using cloud installation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @LaurentP

 

 

if You have a web account, can You go to the dwonload area of the GTAC server?

 

 

regards
Wolfgang

Betreff: standart part installation using cloud installation

Creator
Creator

when i try to connect to:

Training & Support / GTAC Siemens PLM / Download Server /WebKey Login Site

i got this message :

 

"Your WebKey account is valid, but you are not allowed access to this server."

 

it's probably a bad news ......

Highlighted

Betreff: standart part installation using cloud installation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @LaurentP

 

 

so maybe somebody from Siemens can clarify and explain how this is working?

 

It would be interesting how different license types are handled and what could be done by who.

 

regards
Wolfgang