Cancel
Showing results for 
Search instead for 
Did you mean: 

surface to solid...

Valued Contributor
Valued Contributor

Keep'm only asking. ^^
The attached file.
The surface file.
I want to convert it into a solid.

What to do? ... How?

 

5 REPLIES

Re: surface to solid...

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello Hclee,

 

Seems that you open foreign cad/neutral file into solidedge.

 

have you try to open the file into Assembly?

 

if the original / foreign cad/ neutral file you opened is already converted from assembly to part (previous user).

im sure u can use multybody design to make it solid with view steps.

 

Thanks

Re: surface to solid...

Genius
Genius

Hi @Hclee

 

Has an error opening the file, which type of extension opened? I advise you to open the file again in assembly, if the error persists have to rebuild the open surfaces that can generate a solid which leads to more work, otherwise would be the best design from scratch.

 

Thanks.

 

Surface.jpg

Re: surface to solid...

Valued Contributor
Valued Contributor

Thank you~

 

I would like to know the process of conversion to solid.

Did you convert any way?

Re: surface to solid...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Hclee,

 

Do you still have the raw file, that you can post here? [before you opened in Solid Edge] That would be a better place to start to "fix" it.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: surface to solid...

Honored Contributor
Honored Contributor

Sean is right. Just looking at the picture I can see other errors like the right screw head not being correct.