synchronous Stretch

Valued Contributor
Valued Contributor

Hi edge users ..
It is a synchronous feature.
I just selected and dragged the area to reduce it.
An exclamation point occurs.
It's a simple figure that I see ...
Why can not I stretch?

 

 

stretch.png

t is a simple image like the picture.
I can not reduce it.

 


On the other hand, you can move to the face movement function in the net format.
Why is this so?

Traditional.png

Because of these things ...
It's hard to move synchronously.
What is not there?

 

file Attach

 

4 REPLIES

Betreff: synchronous Stretch

Esteemed Contributor
Esteemed Contributor

Hi @Hclee

 

 

 

this behaviour could be explained by te bad and ugly geometry.

 

the upper and lower plane face are not parallel neither is the right cylinder tangent to them (which due to the nonparallel will not be possible)

 

You can - in this state expand the cylinder to the right but there will be a limit shorten it to the left.

 

If You correct this geometry as  I suppose it to be everything works pretty fine.

 

See a picture from the bad end where You can see the non-tangent conditin

 

20170725_1248.PNG

 

 

Setting upper/lower face parallel will solve it.

 



regards
Wolfgang

Betreff: synchronous Stretch

Valued Contributor
Valued Contributor

Thank you for always. Hawcad
This shape is moved from synchronous to modeling after net form.
I do not know when this happened ...
Is there anything that can automatically correct this relationship? ..

Betreff: synchronous Stretch

3D relationships  / face relate tools

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.6

Betreff: synchronous Stretch

Esteemed Contributor
Esteemed Contributor

Hi @Hclee

 

 

see attached video for "How to solve Your issue!"

 

 



regards
Wolfgang