Cancel
Showing results for 
Search instead for 
Did you mean: 

synchronous

Valued Contributor
Valued Contributor

Hi~ Edge users

During the surface command, the split planes feature was used to split the faces.
I want to use a synchronized adjustment wheel to pull the split side 10mm.
But it does not work.
It's a simple task. I wonder why it does not work.

 

split face.png

 

Part file Attach

 

P.S : SOLID EDGE OPTION-->View-->Graphic Cad Setting value

It works differently depending on the graphics card setting value.

 

5 REPLIES 5

Betreff: synchronous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

I'm not quite sure wether I understand Your request correctly, but if it is the "Lift" option while moving the splitted face, what You need,  I'm happy

 

 

See video:

 

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

regards
Wolfgang

Betreff: synchronous

Valued Contributor
Valued Contributor

Oh~

There was a Lift option ... ^^
I always try to catch them as soon as they come out ...
This is why default values are important.
Thanks hawcad

Betreff: synchronous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

one additional statement to this part and the features You have used.

 

 

To move the upper part of the front face doesn't reuest a split surface feature before.

In Sync simply draw a single line from one side to the other and YOu can use the region to lift those piece of face.

 

 And I would be happy to hear wether this will solve Your problem or not.

 

regards
Wolfgang
Highlighted

Re: synchronous

Genius
Genius

Try using the EXTRUDE command as it can work sbetter in some circumstaces.

Re: synchronous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @RLR

 

 

this is what I meant when saying "... there is no need for a split feature ..."

 

Using a sketch line only automatically changes to extrude when using the region

 

But anyway finally there is no difference wether it was a face move with lift or an extrusion to get the wanted results.

 

 

regards
Wolfgang