Cancel
Showing results for 
Search instead for 
Did you mean: 

tutorials

Not applicable

I have 2 computers with v20 installed. Both are windows xp explorer7. On one the
tutorial works fine--but the other the next bar at the top is missing. Any suggestions?
2 REPLIES 2

Re: tutorials

Not applicable

I just installed the latest version of the free software and I have the same problem,
past the first page of all tutorials, there is no NEXT button to use to continue
thru the tutorial. Really makes it impossible to learn to use the software.
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
Robert D. Weaver, Consultant
P.O. Box 515, Heyburn, ID 83336-0515
Voice/Fax (208)679-2690 Field Service 731-2690
robert@brittanysoft.com www.brittanysoft.com

Re: tutorials

Not applicable
Robert,
An ocx failed to register correctly during installation.
Run regsvr32 on hhactivex.dll, most likely located in C:\windows\system32.
So, from the Start -> Run, type the following:

Regsvr32 C:\windows\system32\hhactivex.dll

This should fix the problem.
Regards,
Rick B.