Cancel
Showing results for 
Search instead for 
Did you mean: 

unrolling of a .par

Experimenter
Experimenter

Hello everybody,

 

I´m new with ST7, I learned to use CATIA, so I can´t help to me unroll my constructed figure.

 

May you can help me. It´s a .par

4 REPLIES

Re: unrolling of a .par

might consider this a sheet metal part and "Flatten" 

or, as a part use the blank body command

 

2015-04-02_1133.png

 

 

 

Re: unrolling of a .par

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Muschel, could you attach the part file?

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: unrolling of a .par

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Here is a video what contains similar parts as yours:

 

Important!

Sheetmetal material thickness should be equivalent and you have to be in Ordered mode!

 

Or use what was suggested by @MattJohnsonPAC!

 

BR,

 

Imics
http://solidedgest.wordpress.com/

Betreff: unrolling of a .par

Experimenter
Experimenter

Thanks all of you for your help!

 

With the command flattern of a part I "just" get a surface? Because I want to work (bevelling) at the unrolled part and bend it again.

 

For the moment I´ll try to create my modell as a sheet metall (only with one thickness) , so I think your video will help me a lot.

 

At the moment I´m not able to upload my part, but I will try later.