Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

using a hole pattern to pattern a part in an assembly

Valued Contributor
Valued Contributor

i have a part with a hole feature. that hole feature is then circular patterned. which gives me 3 holes in total.

 

i am now trying to use those holes to pattern a bolt in them holes. but it wont select the holes?

 

can i not select a pattern? does it only work with hole features? 

Regards,

MagRiz
(ST9 User Est 01.18)
13 REPLIES 13

Re: using a hole pattern to pattern a part in an assembly

Gears Phenom Gears Phenom
Gears Phenom

should work just fine,  can you share your part file.

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: using a hole pattern to pattern a part in an assembly

Valued Contributor
Valued Contributor

MagRiz I use this feature sometimes.  It should work.  I tend to skip a step once in a while.  Select the part to pattern in the assembly, then the part that contains the pattern...  Then pick the pattern within this part.  It won't let you pick the original hole.

Betreff: using a hole pattern to pattern a part in an assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

this must work as expected.

 

Try to select another hole instance when selecting the pattern.

Maybe You have got the original base hole feature.

 

 

regards
Wolfgang

Betreff: using a hole pattern to pattern a part in an assembly

Valued Contributor
Valued Contributor

@hawcad @MattS @Johnson_BigMatt

Hi

It doesnt work for me ive made a little video showing the features in the part and then showing what happens when trying to pattern a bolt.

(view in My Videos)

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: using a hole pattern to pattern a part in an assembly

Gears Phenom Gears Phenom
Gears Phenom

@MagRiz   certainly something odd going odd there.   Have you tried to Recompute the Part?

 

RMB on a feature in the PF and select Recompute. 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Betreff: using a hole pattern to pattern a part in an assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

 

can You pack2go this assembly to a zip fiel an d upload here?

 

 

regards
Wolfgang

Betreff: using a hole pattern to pattern a part in an assembly

Valued Contributor
Valued Contributor

@Johnson_BigMatt - i cant seem to find a recompute option

 

@hawcad - i have uploaded the part file you can add it to your own assembly and pattern a bolt. you don't need the other mating part 

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: using a hole pattern to pattern a part in an assembly

Gears Phenom Gears Phenom
Gears Phenom

looks like you are trying to pattern to the mirror, not the pattern.   the "left" (-X) side works as expected.

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Betreff: using a hole pattern to pattern a part in an assembly

Phenom
Phenom

As @Johnson_BigMatt states, the pattern is on the left and the right is a mirror. Place the part and pattern on the left, and then use "clone" to copy all of the features in the right-hand mirrored side. I tested this method and it works fine.

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317