Cancel
Showing results for 
Search instead for 
Did you mean: 

vLookup in Solid Edge Table

Gears Phenom Gears Phenom
Gears Phenom

The disucssion on Displaying a Part variable table in Draft lead to sharing a macro that created a Solid Edge Table from a selection in Excel.

 

I got a couple of PMs if a lookup functionality for Solid Edge tables was also available. A macro for this was already shared in this article last year. Read towards the end of the article about the vLookup functionality in SE tables using the free macro.

 

 

Solid Edge tables do not support zoom to facility through the API so highlighting or zooming in closer to the looked up values is not possible.

 

The macros are attached with this post and any other suggestions for improvement are welcome.

 

Tushar Suradkar

www.SurfAndCode.in

www.CADVertex.com