Cancel
Showing results for 
Search instead for 
Did you mean: 

variable driven values in BOMs

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is there any way to prevent units from showing in a BOM when the values are derived from exposed variables?

If they are not from variables but are instead direct values like mass there is a setting in Options/General to toggle units.

 

Units.JPG

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200
21 REPLIES 21

Re: variable driven values in BOMs

Honored Contributor
Honored Contributor

I do this in a way most people hate on the forum.

 

If I have a sheet metal part. The cutX and cutY must be exposed to make the draft. And parts list displays the gage for the material. the draft of that file displays the part number of the finished part.

 

Then I make an assembly of that single part. Then I assign the part number to the assembly model. That part also no longer displays the cut length and gage, but instead displays the finished part number of that part.

 

Then I only insert the assembly into the next level assembly.

 

This allows me to only have a single place holder for part names and number in every file and allows me to only have a single format for the parts list.

Re: variable driven values in BOMs

Siemens Phenom Siemens Phenom
Siemens Phenom

Bruce,

Is this what you're looking for:

No Units.JPG

Kevin Grayson
Solid Edge Technical Consultant
kevin.grayson@siemens.com

Re: variable driven values in BOMs

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Thanks! I searched the BOM options several times and it was hiding in plain sight the whole time.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: variable driven values in BOMs

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@12GAGE

 

I don't think your post has anything to do with my question but:

 

"This allows me to only have a single place holder for part names and number in every file and allows me to only have a single format for the parts list."

 

Why do you care if you have more than one BOM format? Why not just have a style for each need?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: variable driven values in BOMs

Honored Contributor
Honored Contributor

So that no matter what part is used, it can display in the same parts list. I can use any assembly or part I have without having to think about how the part number flow. My only cost is the sheet metal-assembly bit for parts manufactured in house.

 

From another perspective. I only have one need. To fabricate steel, Sheets, frame, and some "parts"

 

I misread the original question. I thought you were trying to make the numbers not show up at all rather than just without units display.

Re: variable driven values in BOMs

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

The Format... button is easy to lose sight of, since it does not become enabled even if the property text is selected. The button quite strangely is enabled only when clicked inside the text and is still disabled if the cursor is at the end of the text.

 

2016011605.png

 

Re: variable driven values in BOMs

Phenom
Phenom

And of course the Format button does not exist in ST7 or earlier, so you have to add those qualifiers manually.

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.

Re: variable driven values in BOMs

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@12GAGE

"So that no matter what part is used, it can display in the same parts list. I can use any assembly or part I have without having to think about how the part number flow. My only cost is the sheet metal-assembly bit for parts manufactured in house."

 

I still don't understand why different BOM styles won't work for you but I think I'm throwing in the towel.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: variable driven values in BOMs

Honored Contributor
Honored Contributor

I don't understand why anybody would want more than one style of parts list. If you set up your parts for that lists format. Any part can be used on any drawing with the same parts lists. That's how I want it. Path of last resistance/easy.

 

I have very rarely edited my parts lists format over the last year. And only for room, when I do, is typically a permanent change.

 

To me, the goal of the parts list is to assign numbers/names to each component that makes up the result of the drawing. Why would you ever desire more than one list.

 

I can see the need for multiple lists if say, some of the components were for electrical controls or civil concrete & rebar.

 

All I do is steel fabrication drawings and sales drawings. The sales drawing don't include parts lists.