Cancel
Showing results for 
Search instead for 
Did you mean: 

what are units Solid Edge returns using APIs for Mass ?

Experimenter
Experimenter

I want to use APIs to get Mass Properties.

What kind of units Solid Edge API returns for Mass ? In KG,grams ?

 

1 REPLY 1

Re: what are units Solid Edge returns using APIs for Mass ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

For API related questions, check out the following forum:  http://community.plm.automation.siemens.com/t5/Solid-Edge-Developer-Forum/bd-p/SEDeveloperForum

 

To answer your question, the API utilizes the internal unit of measures as follows:

Unit Type Internal Units

DistanceMeter
AngleRadian
MassKilogram
TimeSecond
TemperatureKelvin
ChargeAmpere
Luminous IntensityCandela
Amount of SubstanceMole
Solid AngleSteradian


Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com