what would be the equivalent to pierce relationship,,

Creator
Creator

i have a circle at the end of a line and am trying to pierce it,,, also in sw if i wat to put a plane in the center of 2 faces its a simple as selecting 2 faces and selecting plane,, not having luck with that,, i have been putting a point in the center and then taking the stering wheel to that point is this the shorter way,, thanx for the help,, moneys tight and i cant pay for tutorials,, babby needs a new pair of shoes,, so i have to do everything free and iam going trough alot of bad tutorilas to get to some good ones  

4 REPLIES

I'm not sure what it's called, but you can get it when cr...

MLombard
Retired

I'm not sure what it's called, but you can get it when creating a line, shown in the first image below. The sketch plane is angled, and the endpoint of the line picks up the icon that looks like pierce over the out-of-plane edge.  The bottom image shows the situation when the out-of-plane edge is perpendicular to the sketch plane rather than at some odd angle. Maybe someone can jump in with the correct terminology that I'm missing here.

 

0012.png.

0011.png

Retired Community Manager for Solid Edge. This account is no longer active.

Re: I'm not sure what it's called, but you can get it when cr...

Creator
Creator
thank you,,, i will try it right now

Re: I'm not sure what it's called, but you can get it when cr...

Esteemed Contributor
Esteemed Contributor
It's called a "Pierce Point".

Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: I'm not sure what it's called, but you can get it when cr...

Creator
Creator
i will check it out thanx