Cancel
Showing results for 
Search instead for 
Did you mean: 

why is it so difficult to take a section in the model??

Valued Contributor
Valued Contributor

Comparing to SW, SE is very complicated to take a section. 

 

is there a way to section to a reference plane, i want to avoid going through loads of steps before hand.

Regards,

MagRiz
(ST9 User Est 01.18)
10 REPLIES 10

Re: why is it so difficult to take a section in the model??

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you referring to 3D section views, "Dynamic Section" (Clipping) or the actual Section view?  Or are you talking about 2D section views in Draft?

Do you need a temporary view of a section cut or more permanent for documentation?

Kevin Grayson
Solid Edge Technical Consultant
kevin.grayson@siemens.com

Re: why is it so difficult to take a section in the model??

Valued Contributor
Valued Contributor

Section in the model, i go to the section tool under PMI. not Dynamic Section

 

I just want a section in the model, so i can see what the part looks like when sectioned in model space.

 

 

 

Regards,

MagRiz
(ST9 User Est 01.18)

Re: why is it so difficult to take a section in the model??

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What specifically is so hard about it?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: why is it so difficult to take a section in the model??

Phenom
Phenom

Granted, the PMI section is a few steps long, but you can use it in drawing views etc.

 

However, if you just want to cut away parts quickly, look into the clipping planes function - it's probably the equivalent function to what you were doing in Works.

 

Capture.PNG

Re: why is it so difficult to take a section in the model??

Legend
Legend

I'm not a big fan of section in the model views of PMI, unless I'm wanting to use that on a print.

 

If I'm just wanting to look inside, I prefer to use view clipping, for a temporary use.

Re: why is it so difficult to take a section in the model??

Valued Contributor
Valued Contributor

setting up the section in the first place takes a while. i do like the clip tool though. but most of the times i need to use section as i need to trasnfer that to the drawing. 

 

Regards,

MagRiz
(ST9 User Est 01.18)

Re: why is it so difficult to take a section in the model??

Phenom
Phenom

You can also do a section directly in the draft without doing it in the model....

Re: why is it so difficult to take a section in the model??

Valued Contributor
Valued Contributor

even iso sections?

Regards,

MagRiz
(ST9 User Est 01.18)

Re: why is it so difficult to take a section in the model??

Phenom
Phenom

no, fair point.