Cancel
Showing results for 
Search instead for 
Did you mean: 

wrong dimension presented

Not applicable
Removed and download solid edge 3 times still the software is bugged
when i drawing the basic square within a square 17"x13" square and save next i add
5"x4" then click on distance between add new measurements and enter 4"
then new drawing becomes broken and pushed apart at bottom so that 13" hight become 4" larger and (0 dimension) it pull in a fraction so is less then 17" wide
an see the separtion between square coners the lines do not connect or square is blown apart
4 REPLIES

Re: wrong dimension presented

Not applicable
Do you have Maintain relationships enabled?
Do you see little squares at the endpoints of the four lines that form the
rectangle?
These are the endpoint constraints that hold it together.
Regards,
Rick B.

Re: wrong dimension presented

Not applicable
I do not see squares at the endpoints of the four lines that form the
rectangle it has work with out little quares before and before could not find how get them back

what is Maintain relationships? I only have high school level education

Re: wrong dimension presented

Not applicable
I do not see squares at the endpoints of the four lines that form the
rectangle it has work with out little quares before and before could not find how get them back
what is Maintain relationships? I only have high school level education

"I only have high school level education". Not much of an excuse.
You evidently didn't learn much.
There are plenty of help resources, use them!

Re: wrong dimension presented

Not applicable
On the Home tab there is a there is a Relate command group.
Make sure that the two enabled buttons in the attached image are enabled.
Regards,
Rick B.