Cancel
Showing results for 
Search instead for 
Did you mean: 

Add Feature to Existing Pattern

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

Can a feature be added to an existing Sync part pattern?

Answer

Yes it can...

  1. Click on existing pattern that you want to add feature to from PathFinder
  2. Click on the pattern handle on the part, this exposes Quickbar for the existing pattern feature
  3. Click the Circular, or Rectangular - Add to Pattern button on Quickbar
  4. Select the feature(s) you want to add to the existing pattern then click green check mark
  5. Select the origin with X on it of the original pattern and you should have the additional feature added to the existing pattern
Contributors