Cancel
Showing results for 
Search instead for 
Did you mean: 

Assigning a button to a macro

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

How do you assign a button to a macro like you could in previous versions?

Answer

The ability to assign a button has been intentionally removed. If the programmer has assigned an icon to the command within the code itself, the system will use that icon. The next option is that, if there is a file in the same folder as the macro with the same filename using a .ico, .png or .bmp extension, that file will be used for the icon. As a last resort, the icon assigned to the file type by the operating system will be used.