Showing results for 
Search instead for 
Did you mean: 

Baloon for an Item Number

Siemens Experimenter Siemens Experimenter
Siemens Experimenter


How can I add a balloon that uses the item number defined in the Parts List?


  1. Select the Balloon command
  2. In the Command bar, make sure the button for the option "Link to Parts List" is selected.
  3. Also, select the button for "Item Number" in the Command bar. These options will make sure the item number from the Parts List is added to the balloon.
  4. Click on an edge of the part in which you want to place the balloon. It should show the item number in the balloon.
  5. Click to place.