Cancel
Showing results for 
Search instead for 
Did you mean: 

Base Protrusion Placed as Surface

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

<H2>Question</H2> <P><STRONG>After doing a Part Copy as a Construction in ST5, when I try to create a base protrusion, why is it placing as a surface?</STRONG></P> <H2>Answer</H2> <P>ST5 supports multiple bodies in the Part environment. Adding the protrusion assumes you want to add it to the existing body, which is a surface body. In the far right bottom of the Solids section of the Home tab, click on the Add Body command and then it will allow you to place a new body as a solid.</P>

Contributors