Cancel
Showing results for 
Search instead for 
Did you mean: 

Connecting two conical faces in ST5

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

Why can’t I select a conical face for the Connect relationship in ST5?

Answer

Many improvements were made to the Connect relationship in ST5. To connect two cones, the user must select the vertex at the tip of each cone instead of their faces. Although the workflow is different, the result is the same as in ST4.