Cancel
Showing results for 
Search instead for 
Did you mean: 

Create Filet Weld

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

How do I create a fillet weld in Solid Edge?

Answer

  • To create a fillet weld in asm first toggle the asm to a weldment.
  • This enabled the fillet weld command.
  • On the Features tab select the Fillet weld command.
  • You can set the options on the dialog or dismiss it.
  • Follow the prompts for the command to select faces from components to create the fillet weld between.
  • In the command bar enter the size of the weld bead.
Contributors