Cancel
Showing results for 
Search instead for 
Did you mean: 

Create Frame

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

How do I create a Frame in Solid Edge?

Answer

  • In Assembly go to the tools tab and click frames.
  • This will open the frame environment.
  • Use the wire frame commands or draw a sketch.
  • Run the frame command, select the path and one of the sample frame cross sections.
  • Complete the command to create the frame members.

Note: A warning will appear because you are using a sample frame files. This is OK for learning try out purposes.