Cancel
Showing results for 
Search instead for 
Did you mean: 

Create Piercing in Sheet Metal

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

How can I create a piercing in a synchronous sheet metal part?

Answer

A piercing is basically an operation where the part material is pushed up to shear and open the sides of the feature. This can be easily done with the Punched option of the Bead command.