Cancel
Showing results for 
Search instead for 
Did you mean: 

Create in Place Command Inactive

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

<H2>Question</H2> <P><STRONG>Why is the Create in Place command inactive when editing some subassemblies, but active when editing others?</STRONG></P> <H2>Answer</H2> <P>If Automatic Update is turned off in the subassembly, several commands such as Create in Place, Physical Properties, Assembly Features, etc. will be disabled.</P>

Contributors