Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating a bevel gear from stanrdard gear calculations

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

Is it possible to create a bevel gear from stanrdard gear calculations?

Answer

Yes, you can create bevel gears inside the Assembly enviornment using Engineering Reference functionality. You can also create matching bevel gears with various pitch and diameters.

Comments
Dreamer
Dreamer

I am trying to create a set of miter bevel gears from the Engineering reference and it is not working correctly. These are 32 teeth 6p 20 deg. p.a. gears. For some reason Solid edge wants to make a pinion and a gear and make them different diameters. They both have the same number of teeth, so it is a 1:1 ratio. Can anyone help, or tell me what I'm doing wrong? 

Contributors