Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating a tube like part

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

Is it possible to create a tube like part in Solid Edge?

Answer

Yes, you can do this in the Assembly file using the XpresRoute environment. The Tube command is in XpresRoute and allows you to create paths   between ports/geometry of other components  in the assembly to define   the tube geometry.
Contributors