Cancel
Showing results for 
Search instead for 
Did you mean: 

Distance Between Command Exiting

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

<H2>Question</H2> <P><STRONG>Why does the ‘Distance Between’ command exit in ST5 and not in ST4 with a RMB?</STRONG></P> <H2>Answer</H2> <P>There is new functionality in ST5 called the Solution Manager, which allows you to interact with the model to resolve conflicting relationships. If Auto-Solution Manager is turned on, you are asking Solid Edge to enter the Solution Manager automatically. A Right Mouse Click at this point is designed to exit the Solution Manager and return to the dynamic state. As soon as you place a dimension or when you try moving a face, that is the mode where Solid Edge will take you. To resolve this issue, you can turn off Auto-Solution Manager.</P>

Contributors