Cancel
Showing results for 
Search instead for 
Did you mean: 

Draft File to PDF Quality

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

<H2>Question</H2> <P><STRONG>Why does a Draft file opened in Solid Edge Viewer and then Printed to .PDF have poor quality? </STRONG></P> <H2>Answer</H2> <P>Most likely this can be resolved by the following steps:</P> <UL> <LI>After opening file to print in the viewer, click...Print/Print Preview</LI> <LI>Click Setup, then the Print Layout tab</LI> <LI>Under Quality uncheck the Auto Calculate Print Quality</LI> <LI>Move sliders for Print Image/Preview Image to the right (max.)</LI> <LI>Under Special Settings, select Print as Mono-color, click OK, then print.</LI> </UL>

Contributors