Cancel
Showing results for 
Search instead for 
Did you mean: 

Flipping orientation during part placement

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

Where is the “flip” button located for the mate or align relationships?

Answer

It is not possible to flip the orientation during part placement with mate or align commands. However you can flip the direction for an existing mate or align. Just select the part, select the relationship on the bottom pane. In the ribbon bar that shows up you will see a "Flip" button.

Contributors