Cancel
Showing results for 
Search instead for 
Did you mean: 

How to Control Round Off With Dimensions in Solid Edge

Experimenter
Experimenter
How to Control Round Off with Dimensions/Callouts

Step 1:   Select the Hole Callout that you need the round off changed.  Notice what style this callout is using.

 

Step 2:   This callout is using the default style, ANSI (inch).  The style is what drives the round off for the Callout.

 

Step 3:   To edit the style:

a.   Click on Styles

b.   Dimensions should be highlighted by default

c.   Highlight the style that we noticed above in step 2.  Click Modify... 
d.   Click on the Units tab

e.   Notice the Round-off value.  Edit this value.

f.    Click OK.  You can click Apply to apply this change to all dimensions/callouts that are using that style.

 

*Note:  All the Dimensions/callouts that use that style (in this example ANSI (inch)) will change to the new round-off.  If you need one dimension or callout that needs a different round-off value, you will need to create a different style.
 
To Create A New Style Based On The Existing
Step 1: Click Styles.  Click New...

 

Step 2:   Give this style a name which you recognize.  I called this Ansi_roundoff_6 for example.

 

Step 3:   Now I can click on the Units tab and pick the round-off to be 6 places.

 

Step 4:   Click Ok.  You now see that style created and in the list.  Click Close.

 

Now you can add your new callout with that Style or change an existing callout to the new style.

To change the style on an existing callout, select the callout with your select tool.  Then select the new Ansi_roundoff_5 style from the drop down list.  The callout will update with the proper round-off.

 

For a step-by-step with images, go here
Contributors