Cancel
Showing results for 
Search instead for 
Did you mean: 

Meeting GOST Standards: with Symbol Line Thickness Support for GOST Weld Symbol

Siemens Dreamer Siemens Dreamer
Siemens Dreamer

 

As per the GOST standards, permanent joint symbols should have thicker line representation. To accomplish this behavior, Solid Edge 2019 enriched GOST weld symbol to support a separate line thickness for the permanent joint symbols as shown below.

1.png

ANSI/ISO weld symbol already supports a thicker line representation where “Symbol line width” dimension style parameter controls line width thickness separately. It can also be overridden from ‘Text and leader’ properties page.

 

2.png

 

The same dimension style parameter is supported for GOST weld symbol and exposed on ‘Text and leader’ properties page.

 

3.png

 

When symbol line width is changed, the line width is changed for permanent joint symbols only. This is supported for both draft and PMI GOST weld symbol. Pixel size PMI doesn’t honor this symbol line width parameter.

 

Below is an example of permanent joint symbols honoring symbol line width parameter.

 

4.png

 

To summarize, symbol line thickness support allows displaying thicker line representation for permanent joint symbols. This enhancement greatly improves the experience of using GOST weld symbols in Solid Edge.

Contributors