Cancel
Showing results for 
Search instead for 
Did you mean: 

Model Type Field Empty

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

Why is the Model Type field empty in Property Manager for some files but not for others?

Answer

The Model Type column in Property Manager is used to show if the part file is a Synchronous or Ordered model. For ST and ST2 files, the field should show either value, but for ST3 and later releases, this field will be empty as a part file can contain both Synchronous and Ordered features, so a model type cannot be defined.