Cancel
Showing results for 
Search instead for 
Did you mean: 

New Feature Shown as Construction

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

Why does a new feature show as construction after an insert part copy with Copy as Construction option?

Answer

The introduction of multi-bodies in ST5 triggered this behavior. The protrusion is being added to the construction body, as designed. User may use “Add New Body” to create in a manner similar to ST4 and previous versions. After this command is used, the features are added to a different body, which is the expected behavior.