Cancel
Showing results for 
Search instead for 
Did you mean: 

Place Components in Assembly

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

How do I create an Assembly and place components in it?

Answer

You create a new assembly (asm) by running file new and selecting an asm template.

  • Use the parts library tab (vertical tab on the left) to select a component to place.
  • Drag and drop the selected component into the asm.
  • You can also drag and drop a Solid Edge 3D model file (*.par, *.psm, *.asm) from windows explorer into the asm.
  • The first component is grounded (fixed) relative to the asm origin.
  • Drag and drop additional components as needed.

Use the files in the Training folder located in the Solid Edge installation folder to get started.

Contributors