Cancel
Showing results for 
Search instead for 
Did you mean: 

SEU13: 411 - Creating Exploded and Animated Assemblies - Steve Webb

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Steve Webb, Solid Edge Field Support, Siemens PLM Software 

In this session we will take a deep drive into the two different ways a user can create an exploded assembly and which method is the correct way for the output that is needed. The Solid Edge Explode Rendering Animate (ERA) environment has many tools to allow you to create the perfect explosion of your designs, and all of these tools will be covered. Once the exploded model has been created, we'll then cover how to animate it. If you need to create exploded drawings, or show how your designs are assembled or dissembled, this is a must attend session.

Contributors