Cancel
Showing results for 
Search instead for 
Did you mean: 

SEU13: 503 - Taking Solid Edge Sheet Metal to the Next Level Advanced Topics - Jeff Walker

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Jeff Walker - Sheet Metal, Sketching and Modeling Technology, Siemens PLM Software

This course will introduce advanced sheet metal features in Solid Edge and the integrated modeling environment. Users will be exposed to the concepts of how the two distinct modeling systems work together in a single file; either part file or sheet metal file. Integrated modeling proposes new ways of design and this class will explore these advances. Synchronous users that attend this class will learn about the powerful ordered features and when to use them. Traditional users will be exposed to the synchronous environments so that they may understand when to convert their systems, models, or features to the new paradigm. Workflows will include pure synchronous models vs. integrated models, Live Sections and sketches, and transforming designs to synchronous.

Contributors