Cancel
Showing results for 
Search instead for 
Did you mean: 

Setting thickness and bend radius for a Sheet Metal part

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Question

How do you set the thickness and bend radius for a Sheet Metal part?

Answer

Use the Gage tab on the Material Table dialog in Sheet Metal to set the part thickness and bend radius. The Material Table command can be accessed from the Properties menu on the Application Button located in the upper left corner of the application.
Contributors